Skip to main content
Knowledgebase
Home
Renesas Singapore - Knowledgebase

TPS-1 Stack Code Protection

Last Updated:06/01/2017

Question:

Is there any method of protection to prevent others from copying the TPS-1 stack code?

Answer:

The TPS-1 stack code is stored on external serial flash without encryption, so there is no protection from others downloading the stack. However the TPS-1 PROFINET stack is freely available for download on the internet and there is no reason anyone would need to go through the effort of acquiring the stack code in this way. Customers should focus on the code protection on the MCU side to prevent their custom code from being cloned by others.
Suitable Products
TPS-1