Skip to main content
Knowledgebase
Home
Renesas Singapore - Knowledgebase

One pipe register used for host function & peripheral function?

Latest Updated:02/01/2009

Question:

When using the host function (port 1) and peripheral function (port 2) of the USB host/peripheral controller at the same time, can one pipe register be used for both functions?

Answer:

No, it cannot. One pipe register must be used for one function.
Suitable Products
D/A Converters