Skip to main content
Knowledgebase
Home
Renesas Singapore - Knowledgebase

Does USB peripheral function of UPD720150 support low speed transfer?

Latest Updated:02/01/2009

Question:

Does the USB peripheral function of the UPD720150 support low-speed transfer?

Answer:

No; data can only be transferred in high-speed or full-speed mode.
Suitable Products
Serial Communication Controller