Skip to main content
Knowledgebase
Home
Renesas Singapore - Knowledgebase

What's the difference of “Max.” and “Typ.” for asynchronous SRAM?

Latest Updated:03/16/2012

Question:

Please explain the difference between “Max.” and “Typ.” standby current in the datasheet for asynchronous SRAM.

Answer:

”Max.” is the maximum guaranteed value.
“Typ.” is a reference value that is the average value of some samples.
The “Typ.” value is not guaranteed.
Suitable Products
Asynchronous SRAM