Skip to main content
Knowledgebase
Home
Renesas Singapore - Knowledgebase

What are the differences between the H8/3834 and H8/3834S ?

Latest Updated:03/18/2009

Question:

"What are the differences between the H8/3834 and H8/3834S ?

Answer:

The H8/3834S is a pin and function compatible die shrink version of the H8/3834. Due to the shrink process the device has significantly improved power consumption compared to the original devices.However the die shrinking process also results in different EMC characteristics and so for products where EMC performance is an issue, careful evaluation of the S version should be carried out.
Suitable Products
H8/300L