Skip to main content
Knowledgebase
Home
Renesas Singapore - Knowledgebase

What will happen if these outputs MTU, MMT, OCSR is in high active state?

Latest Updated:03/26/2009

Question:

Output Short Flag of MTU, MMT, OCSR indicates that among the three pairs of 2 phase

outputs compared, the outputs of at least one pair have simultaneously become Low level

output. In this case, when the output is in the Low active state, output shut-down is possible only when the timer output simultaneously becomes Low level. However, what will happen if the output is in the High active state?

Answer:

Answer
Suitable Products
SH7065