Skip to main content
Knowledgebase
Home
Renesas Singapore - Knowledgebase

What mode is possible to specifying areas with different bus width?

Latest Updated:03/26/2009

Question:

Is it possible to specifying areas with different bus width for the source address and destination address?

Answer:

It is possible to specifying areas with different bus width for the source address and destination address in Dual address mode.
It is impossible in Single address mode.
Suitable Products
SH7700 Series
SH7729R
SH7727
SH7709S
SH7706
SH7705