Skip to main content
Knowledgebase
Home
Renesas Singapore - Knowledgebase

What are the differences in specification between SH7615 and SH7616?

Latest Updated:03/23/2009

Question:

What are the differences in the specification between SH7615 and SH7616?

Answer:

SH7616 adds the following improvements to SH7615:

  • FIF0 size for Ethernet: extended from 512Byte to 2048Byte for transmit/receive, respectively.
  • Support for CAM match signal
  • Added 1 channel of SIOF(FIFO internal serial interface).
Please refer to the following document for details.
Specification comparison between SH7615 and SH7616
SH7615 and SH7616 are full-pin compatible in the same package product (QFP-208).
Suitable Products
SH-Ether
SH7616
SH7615