Is the address error handling CPU when E-DMAC address error occur?
Latest Updated:03/26/2009
Question:
Is address error exception handling(CPU address error or DMA address error) generated when E-DMAC address error is occurred (ADE bit of EtherC/E-DMAC status register(EESR) is set)?
Answer:
When E-DMAC address error is occurred, address error exception handling is not generated.
When ADE bit is set under the condition that ADEIP bit (Address error interrupt permission) of EtherC/E-DMAC status interrupt permission register (EESIPR) is set to "1", EINT0 interruption is generated.
Suitable Products
SH7710 |
SH7619 |
SH7618 |