Skip to main content
Knowledgebase
Home
Renesas Singapore - Knowledgebase

Is it possible to rewrite the MMT_TCNT while MMT is being counted?

Latest Updated:03/26/2009

Question:

Is it possible to rewrite the MMT_TCNT (timer counter) while MMT (motor management timer) is being counted?

Answer:

Rewrite the timer counter of MMT after timer counter is stopped.

Please refer to the following technical update for stopping the timer counter of MMT.
http://documentation.renesas.com/eng/products/mpumcu/tu/tnsh7a551ae.pdf

Suitable Products
SH7065
SH7047, SH7049, SH7105, SH7107, SH7109
SH7046, SH7148, SH7101, SH7048, SH7104, SH7106, SH7108