Skip to main content
Knowledgebase
Home
Renesas Singapore - Knowledgebase

Is it OK to put wait state using WAIT pin if CS2/3 spaces linked to SDRAM?

Latest Updated:03/25/2009

Question:

Is it possible to insert the wait state by using the WAIT pin, when CS2 space or CS3 space are connected to the SDRAM?

Answer:

The wait state is not inserted by using the WAIT pin for SDRAM space. Access cycle numbers for SDRAM space are adjusted by setting CAS latency, pre-charge completion wait cycle numbers and others in the Bus State Controller(BSC). Please refer to the hardware manual of each product for the setting detail.
Suitable Products
SH7729R
SH7727
SH7720
SH7709S
SH7706
SH7705