Skip to main content
Knowledgebase
Home
Renesas Singapore - Knowledgebase

Is it OK to do three phase output without the dead time using MMT?

Latest Updated:03/26/2009

Question:

Is it possible to perform the positive phase three phase output without the dead time using MMT (motor management timer) ?

Answer:

Answer
Suitable Products
SH7060 Series
SH7065
SH7047 Series
SH7046 Series