Skip to main content
Knowledgebase
Home
Renesas Singapore - Knowledgebase

Is interrupt from other built-in module accepted amid block transfer?

Latest Updated:03/25/2009

Question:

Is the interrupt from other built-in peripheral modules accepted during block transfer?

Answer:

During block transfer, the interrupt from other peripheral modules cannot be accepted. After one block transfer, the interrupt will be accepted.
Suitable Products
SH7144, SH7145
SH7046, SH7148, SH7101, SH7048, SH7104, SH7106, SH7108
SH7040, SH7041, SH7042, SH7043, SH7044, SH7045