Skip to main content
Knowledgebase
Home
Renesas Singapore - Knowledgebase

Is CS0 output even when built-in ROM is accessed?

Latest Updated:03/23/2009

Question:

In case of built-in ROM effective mode, even when built-in ROM is accessed, is CS0 output?

Answer:

CS0 becomes effective only when the CS0 space range is accessed. Because built-in Rom is not a CS0 space, CS0 is not output. Please refer to "Pin States" in the appendix of the hardware manual.
Suitable Products
SH7065
SH7058
SH7055
SH7018