Skip to main content
Knowledgebase
Home
Renesas Singapore - Knowledgebase

IRQ interrupts: input bus release state retained until CPU takes back?

Latest Updated:03/25/2009

Question:

Are IRQ interrupts input in the bus release state retained until the CPU takes back the bus mastership?

Answer:

- If IRQ interrupts are set to edge detection
IRQ interrupt requests are retained.


- If IRQ interrupts are set to level detection
IRQ interrupts are not generated, while the IRQ pin is negated.
To accept IRQ interrupt requests, it is necessary to keep the level of the IRQ pin effective until the CPU takes back the bus mastership(until interrupts are accepted).

Suitable Products
SH7144, SH7145
SH7065
SH7058
SH7055
SH7050, SH7051
SH7052, SH7053, SH7054
SH7047, SH7049, SH7105, SH7107, SH7109
SH7040, SH7041, SH7042, SH7043, SH7044, SH7045
SH7032, SH7034, SH7034B
SH7032
SH7020, SH7021