Skip to main content
Knowledgebase
Home
Renesas Singapore - Knowledgebase

How is SH767x Ethernet transfer speed?

Latest Updated:09/28/2009

Question:

How is SH767x Ethernet transfer speed?

Answer:

Ethernet transfer speed depends on driver software, the TCP/IP protocol stack software, and evaluation conditions. The following maximum speeds were observed during testing by Renesas. They are provided as reference values only, and are not guaranteed.

TCP Write
48.7 Mbps
TCP Read
55.1 Mbps
UDP Write
70.8 Mbps
UDP Read
73.0 Mbps
Suitable Products
SH7670