Skip to main content
Knowledgebase
Home
Renesas Singapore - Knowledgebase

Do wait cycles inserted if data transfer to external memory using DMAC?

Latest Updated:03/25/2009

Question:

Are wait cycles inserted, when performing data transfer to the external memory by using the DMAC?

Answer:

-Dual Address Mode
Wait cycles for each CS space specified by the Wait Control Register1(WCR1) of the Bus State Controller(BSC) are inserted.

-Single Address Mode
Wait cycles for each CS space(or DRAM space) specified by the Wait Control Register2(WCR2) of the Bus State Controller(BSC) are inserted.

Suitable Products
SH7144, SH7145
SH7050, SH7051
SH7040, SH7041, SH7042, SH7043, SH7044, SH7045
SH7014, SH7016, SH7017