Skip to main content
Knowledgebase
Home
Renesas Singapore - Knowledgebase

Can the crystal resonator be used as the clock for USBH/USBF of SH7720?

Latest Updated:03/23/2009

Question:

Can the crystal resonator be used as the clock (48MHz) for USBH/USBF of SH7720?  In addition, is there any recommended crystal resonator?

Answer:

The crystal resonator can be used as the clock (48MHz) for USBH/USBF of SH7720.

There is not any special recommended crystal resonator from Renesas Electronics.

Please consider to choose it with getting the evaluation of the resonator makers.

Suitable Products
SH7720