Skip to main content
Knowledgebase
Home
Renesas Singapore - Knowledgebase

RZ/T1 Analog Pins Connected to VCCQ33 with Pull-up Resistor

Last Updated:09/27/2017

Question:

Is it possible to connect the analog pins (AN000 to AN007) to VCCQ33 with a pull-up resistor?   Even though, in User's Manual: 17.4 Handling of Unused Pins, it says these analog pins should be connected to AVSS0 with a pull-down resistor?

Answer:

Yes, it is possible. If analog pins AN000 to AN007 are not used, these pins can be connected to VCCQ33 with pull-up resistor.
Suitable Products
RZ/T1
  • Was this article helpful?