Skip to main content
Knowledgebase
Home
Renesas Singapore - Knowledgebase

Problems with Slow Rising and Falling Input Signals

Last Updated:09/27/2017

Question:

Is there a problem if an input signal rises or falls gradually?

Answer:

Potentially. If an input signal rises or falls gradually, it is easily influenced by noise and, as a result, could affect a high/low level decision. Additionally, it is more likely to conduct a shoot-through current because the input level is floating at the intermediate position.

Although there is no specification, it is recommended to avoid slow rises and falls in input signals.

Suitable Products
RZ/T1
  • Was this article helpful?