Skip to main content
Knowledgebase
Home
Renesas Singapore - Knowledgebase

Missing Parameters for the Loader in External Flash

Last Updated:09/27/2017

Question:

What happens if the parameters for the loader are not written in the external flash memory?

Answer:

The errors "Checksum error of the parameters for the loader" or "Error in a parameter for the loader" will occur and the CPU will go into a infinite loop during boot processing.  Also, the error information is stored in the dedicated address of "0080 09C4h".

For more details, refer to the RZ/T1 Group User’s Manual: Hardware (R01UH0483) "3.5.7 Boot-Related Information and Error Processing."

Suitable Products
RZ/T1