Skip to main content
Knowledgebase
Home
Renesas Singapore - Knowledgebase

How many levels of USB hubs can be connected in cascade to one USB 2.0 host port?

Latest Updated:05/09/2016

Question:

How many levels of USB hubs can be connected in cascade to one USB 2.0 host port?

Answer:

As per the USB specifications, up to 5 levels of hubs can be cascaded together.
Suitable Products
RZ/G
  • Was this article helpful?