Skip to main content
Knowledgebase
Home
Renesas Singapore - Knowledgebase

Can a pull-up resistor built into the IO be switched on and off by a register?

Latest Updated:05/09/2016

Question:

Can a pull-up resistor built into the IO be switched on and off by a register?

Answer:

The Pin Function Controller (PUPRx) can be used for switching on and off. For details, please see the documentation for each product (Specifications of Individual RZ/G Series Product). 
Suitable Products
RZ/G
  • Was this article helpful?