Skip to main content
Knowledgebase
Home
Renesas Singapore - Knowledgebase

Built-In Cache for Cortex-M3 of RZ/T1

Last Updated:09/27/2017

Question:

Is there a built-in cache in the Cortex-M3 of the RZ/T1?

Answer:

No, there is not. Built-in cache is only available in the Cortex-R4.
Suitable Products
RZ/T1