Skip to main content
Knowledgebase
Home
Renesas Singapore - Knowledgebase

What is the status of the pins during reset and standby?

Latest Updated:06/20/2013

Question:

What is the status of the pins during reset and standby?

Answer:

Please refer to the Appendix "Port States in Each Processing Mode" of the hardware manual.
Suitable Products
RX62N, RX621
RX62T
RX610
RX62G
RX630
RX63N, RX631
RX63T
RX210
RX220
RX110
RX111