Skip to main content
Knowledgebase
Home
Renesas Singapore - Knowledgebase

What happens if the data that you want to program is FFFFh?

Latest Updated:05/27/2013

Question:

In subsection (2) of the FCU Commands section of the Data Flash (Flash Memory for Data Storage) chapter of the user's manual: hardware, it states that "If the area accessed... includes addresses that do not require programming, write FFFFh as the programming data for those addresses." What if the data that you want to program is FFFFh?

Answer:

If the data that you want to program is FFFFh, write FFFFh.
Suitable Products
RX62N, RX621
RX62T
RX610