Skip to main content
Knowledgebase
Home
Renesas Singapore - Knowledgebase

What document must I refer the states needed to execute instructions?

Latest Updated:06/20/2013

Question:

The user's manual: software does not mention the number of states necessary to execute each instruction.
Which document should I refer to for this information?

Answer:

For the number of cycles for instructions, please refer to Instructions Converted into Single Micro-Operation and Instructions Converted into Multiple Micro-Operations in the Instructions and Pipeline Processing section in the product's user's manual: hardware.
Suitable Products
RX62N, RX621
RX62T
RX610
RX630
RX63N, RX631
RX210
RX220
RX110
RX111