Skip to main content
Knowledgebase
Home
Renesas Singapore - Knowledgebase

Target of the new RX130 group

Last Updated:01/29/2018

Question:

For what kind of application is the new RX130 touch suitable?

Answer:

Featuring a new capacitive touch IP with improved sensitivity and robustness, and a comprehensive device evaluation environment, the new 32-bit RX130 MCUs are an ideal fit for devices designed with challenging, non-traditional touch materials, or required to operate in wet or dirty environments, such as a kitchen, bath, or factory floor.
Suitable Products
RX130