Skip to main content
Knowledgebase
Home
Renesas Singapore - Knowledgebase

Rewriting flash memory returning from deep software standby?

Latest Updated:06/20/2013

Question:

After entering and then returning from deep software standby, the flash memory cannot be rewritten.
Why?

Answer:

FCURAM is undefined after entering deep software standby. Thus, it is necessary to download FCURAM from FCUROM again after returning from deep software standby.
Suitable Products
RX62N, RX621
RX62T
RX610
RX630
RX63N, RX631
RX210