Skip to main content
Knowledgebase
Home
Renesas Singapore - Knowledgebase

Can I connect the VCL pin to VCC?

Latest Updated:01/23/2014

Question:

Can I connect the VCL pin to VCC?

Answer:

Please do not connect the VCL pin to VCC. The VCL pin is the connector pin for the smoothing capacitor for stablilizing the internal power supply. As described in the manual, please connect it to VSS via a 0.1 uF capacitor.
Suitable Products
RX630
RX63N, RX631
RX210