Skip to main content
Knowledgebase
Home
Renesas Singapore - Knowledgebase

Monitor Communication Between MCU's with Wireshark

Last Updated:06/08/2017

Question:

Can I monitor communication between MCU boards using Wireshark?

Answer:

Yes.  You can use HUB with a port mirroring function, then all the packets passing through the HUB will be output by the port that's been set for mirroring. You can monitor communication between MCU boards by connecting that port with a PC operating Wireshark.
Suitable Products
RX62N
RX63N
RX65N
RX64M
RX71M
  • Was this article helpful?