Skip to main content
Knowledgebase
Home
Renesas Singapore - Knowledgebase

When another activation factors occur during DTC transfer

Last Updated:01/16/2018

Question:

How will the DTC operate if an activation source with a higher priority than the current activation source is generated during the current DTC transfer ?

Answer:

When an activation source that has a higher priority than the current activation source is generated during a DTC transfer, the newly generated DTC activation source is put on hold until the current DTC transfer is completed. After the current transfer request is completed, the DTC is activated by the newly generated activation source.
Suitable Products
RL78/F13
RL78/F14
RL78/F15
RL78/G14
  • Was this article helpful?