Skip to main content
Knowledgebase
Home
Renesas Singapore - Knowledgebase

Is it all right not to define the corresponding interrupt function?

Latest Updated:08/01/2001

Question:

Since no interrupt servicing is required at this time, is it all right not to define the corresponding interrupt function?

Answer:

Yes, it is not necessary to define the interrupt function.
Suitable Products
RL78 Family
78K Family