Skip to main content
Knowledgebase
Home
Renesas Singapore - Knowledgebase

Does reset pin input has the same result if reset occurs due to overflow?

Latest Updated:12/01/2011

Question:

If a reset occurs due to overflow in the "reset operation upon overflow" mode, does the same operation as /RESET pin input result?

Answer:

Yes, this is correct.
For details, refer to the "Reset Function" section in the User's Manual.
Suitable Products
RL78 Family
78K Family