Skip to main content
Knowledgebase
Home
Renesas Singapore - Knowledgebase

Description of initial settings of internal peripheral I/O

Last Updated:12/26/2017

Question:

Initial settings of internal peripheral I/O are described to the hdwinit function. Can't it be described elsewhere?

Answer:

Basically, initial settings of the internal peripheral I/O may be described anywhere as long as they are described before the internal peripheral I/O is actually used.

If initial settings of a port that is to be set in the output mode are late, the influence of noise may increase.
In addition, the operating clock operates at a low frequency in the default status.
Completing initial settings as soon as possible is recommended, taking the relationship between the supply voltages and operating clock frequency into consideration.
Moreover, manipulating the setting of the watchdog timer after the execution program has been started is not recommended.

Suitable Products
RL78 Family
78K Family