Skip to main content
Knowledgebase
Home
Renesas Singapore - Knowledgebase

About software trigger mode of A/D converter

Last Updated:01/16/2018

Question:

Where is the "conversion time" in the figure "Timing Chart When A/D Voltage Comparator Is Used" below when the A/D converter is used in software trigger mode?
When is the voltage value at the analog input pin obtained?

Answer:

The "conversion time" in software trigger mode refers to the "conversion operation" in the timing chart. The voltage value at the analog input pin is obtained when the A/D converter starts its operation after the conversion activation time has passed [during the period of sampling (number of sampling clocks: 5 fAD or 7 fAD)].

2000462_e.png

Suitable Products
RL78/F12
RL78/F13
RL78/F14
RL78/F15
RL78/D1A
RL78/G13
RL78/G14
  • Was this article helpful?