What is the reason why the system enters the wait status?
Latest Updated:12/01/2011
Question:
Even if there is enough space available, when get_blk is executed, the system enters the wait status.
Is there any way of analyzing the cause of this?
Is there any way of analyzing the cause of this?
Answer:
Use the task debugger (RD850 Pro) in a case like this.
You can check the wait status of the memory pool using the RD850 Pro.
You can check the wait status of the memory pool using the RD850 Pro.
Suitable Products