Skip to main content
Knowledgebase
Home
Renesas Singapore - Knowledgebase

What to do if the products not listed in the CISTEC released list?

Latest Updated:12/01/2006

Question:

Regarding products not listed in the CISTEC released list, what should be done?

Answer:

Obtain the parameter sheet from the distributor where you purchased your product and submit it to the customs agent.
Note, however, that products exempt from export regulations do not require an export certificate. Parameter sheets are therefore not available for these products.
Suitable Products