Skip to main content
Renesas Singapore - Knowledgebase

What are the specifications of USB 2.0 of Renesas Electronics?

Latest Updated:08/01/2005


What are the specifications of the USB 2.0 host controllers of Renesas Electronics?


Up to five USB ports are provided.
Each port can be connected to USB devices of different speeds, i.e. HS (480 Mbps), FS (12 Mbps), and LS (1.5 Mbps).

Furthermore, our USB 2.0 host controllers also provide one EHCI host controller core and two OHCI host controller cores.
On the system side, a PCI bus (PCI 2.2 standard compliant) is provided, allowing direct connection to the PCI bus.

Suitable Products