Skip to main content
Knowledgebase
Home
Renesas Singapore - Knowledgebase

Application of RL78/G1D module (RY7011) firmware to end-products

Last Updated:09/20/2017

Question:

Can firmware written at shipment of the RL78/G1D module (RY7011) be applied directly to the end-product without being rewritten?

Answer:

Factory firmware at shipment can be applied to end-products as it is. However, since the written firmware is the positioning of the firmware for operation confirmation, please use it after sufficient evaluation at time of productization.

RL78/G1D Module Firmware User's Manual (R01UW0160)
https://www.renesas.com/search/keyword-search.html#q=R01UW0160&genre=document

Suitable Products
RL78/G1D
Bluetooth