Skip to main content
Knowledgebase
Home
Renesas Singapore - Knowledgebase

"GUI tool" Supported Windows Version

Last Updated:09/20/2017

Question:

The Bluetooth® Low Energy Protocol Stack GUI tool is described to work with Windows 7 SP1 in the operating environment portion of the application note, but will it work on Windows 10?

Answer:

The Bluetooth® Low Energy Protocol Stack GUI tool can be used with Windows 10. It's operation has been confirmed and a corresponding notation in application note will be changed at the next revision.

Bluetooth® Low Energy Protocol Stack GUI Tool (R01AN2469)
https://www.renesas.com/search/keyword-search.html#q=R01AN2469&genre=tooldownload

Suitable Products
RL78/G1D
Bluetooth
  • Was this article helpful?