Skip to main content
Knowledgebase
Home
Renesas Singapore - Knowledgebase

Bluetooth SIG Qualification Status if Bluetooth module of previously qualified product is changed

Last Updated:02/13/2017

Question:

Is Bluetooth SIG re-qualification required when changing the Bluetooth module within a product?

Answer:

If you change to the Bluetooth module with different qualified design, you will need to re-qualify.
A declaration fee (8,000 USD for Adopter level members) is required for re-qualification.

Suitable Products
RL78/G1D
Bluetooth