Skip to main content
Knowledgebase
Home
Renesas Singapore - Knowledgebase

Notes on C/C++ Compiler Package & R8C Family V.6.xx Release xx

Latest Updated:06/27/2011

Question:

I was using an earlier version (V.5.45 Release 01 or earlier) C Compiler Package for M16C Series and R8C Family [M3T-NC30WA].

I will start to use C/C++ Compiler Package for M16C Series and R8C Family [M3T-NC30WA] V.6.xx Release xx and I am looking for documentation that offers notes or instructions pertaining to the new version compared to the old version as well as how to migrate user applications to the new version.

Answer:

C/C++ Compiler User's Manual comes with the "Appendix K Contents of Upgrade and Migration Method."
Download the C/C++ Compiler User's Manual here.
Suitable Products
C/C++ Compiler Package for M16C Series and R8C Family [M3T-NC30WA]