Skip to main content
Knowledgebase
Home
Renesas Singapore - Knowledgebase

How to change VDD by the RL78 peripheral module simulator

Last Updated:06/21/2017

Question:

I am using the RL78 peripheral module simulator. How can I change the VDD voltage?

Answer:

There is a way to change the VDD voltage by the RL78 peripheral module simulator. Create a level gauge and specify VDD for the connection pin. If you want to set the VDD voltage to 3.3 V, you can change the VDD voltage to 3.3 V by setting the level gauge value to 3300 mv.
Suitable Products
e² studio
CS+ (formerly CubeSuite+)
Simulator