Skip to main content
Knowledgebase
Home
Renesas Singapore - Knowledgebase

How can I measure an execution time for the specified interval?

Latest Updated:12/15/2014

Question:

How can I measure an execution time for the specified interval?

Answer:

To measure an execution time for the specified interval, please set on each pane as below.

Cycle counts are shown on the panes.
Please divide the cycle counts by frequency of the main clock to measure an execution time.
For the details of other options and the way to set them, see at  "e2 studio Trace" and "e2 studio Performance Analysis View" in the e2 studio Help.
Suitable Products
e² studio