Skip to main content
Renesas Singapore - Knowledgebase

Which is better E1 or E20 for RAM monitoring when debugging program?

Latest Updated:11/25/2014


How do I use the RAM monitoring facility (to view contents of memory while a program is running) when using the E1 or E20 to debug a program for an RX family microcontroller under the CubeSuite+?
Is there any difference in performance between the E1 and E20?


Although both the E1 and E20 have RAM monitoring facilities, they differ on points such as the times over which the user program is halted and the way to set up the facilities under the CubeSuite+.
For details, refer to the following document.
RAM Monitoring Facility of CubeSuite+ for RX (rx_qs_RAM_monitor-e_141001.pdf: 579 KB)
Suitable Products
RX Family
CS+ (formerly CubeSuite+)
E1 [R0E000010KCE00]
E20 [R0E000200KCT00]