Skip to main content
Knowledgebase
Home
Renesas Singapore - Knowledgebase

When I use CS+ for CA, CX, to which manual should I refer?

Last Updated:04/26/2017

Question:

When I use CS+ for CA, CX, to which manual should I refer?

Answer:

Refer to the following manuals for CubeSuite+. For 'CubeSuite+', read 'CS+'.

Contents Manual for reference
Installing CubeSuite+ CubeSuite+ User's Manual: Start
Manipulating a project CubeSuite+ User's Manual: Start
Code generator tool* CubeSuite+ User's Manual: Design
Editor CubeSuite+ User's Manual: Coding and Debug
Build tool CubeSuite+ User's Manual: Build
Debug tool CubeSuite+ User's Manual: Debug
Program analyzer CubeSuite+ User's Manual: Analysis
Python console CubeSuite+ User's Manual: Start
Updating CubeSuite+ CubeSuite+ User's Manual: Start
Message CubeSuite+ User's Manual: Message


*For the RL78 code generation tool, refer to the manual of CS+ for CC.

For details, go to :Information on Support by CS+.

Suitable Products
CS+ (formerly CubeSuite+)