Skip to main content
Knowledgebase
Home
Renesas Singapore - Knowledgebase

Specifying the compile option for each file on CS+

Last Updated:05/24/2017

Question:

How do I specify the compile option for each file on CS+?

Answer:

Select a file in the Project Tree panel, and then the property from the right-click menu.

In the Build Settings tab in the Property panel for each file,

select “Yes” for “Set individual compile option” in "Build".

This allows you to set the compile option for each file.

Suitable Products
CS+ (formerly CubeSuite+)