Skip to main content
Knowledgebase
Home
Renesas Singapore - Knowledgebase

Measuring performance of RH850/F1L CS+

Last Updated:09/20/2017

Question:

Is it possible to measure the performance of the program of RH850/F1L with the E1 emulator?
I want to measure the time between two points.

Answer:

For RH850/F1L, the time between two points can be measured, and the hot pug-in function is available with the E1 emulator in conjunction with IDE CS+ V3.01.00 or later.

Refer to the following user’s manual for setting.
  Integrated Development Environment User’s Manual: RH850 Debug Tool
  2.14.1 Measure the performance in a section

The performance can also be measured by using the E2 emulator.
 

Suitable Products
CS+ (formerly CubeSuite+)
E1 Emulator