Skip to main content
Knowledgebase
Home
Renesas Singapore - Knowledgebase

Is CubeSuite+ change setting required for switching MCU and ROM set up?

Latest Updated:10/29/2014

Question:

When switching between target MCUs, in addition to changing the setting for ROM capacity, do I need to change settings such as the environment settings for CubeSuite+ ?

Answer:

After you have changed the target microcontroller for a project in the CubeSuite+ environment, change the following setting.

In [Property] of the CC-RX (build tool), change the setting for [Section] -> [Section start address] on the [Link Options] tabbed page to suit the ROM or RAM space of the CPU you will be using.
In CS+ 3.00.00 and later versions, the section start addresses allocated by default correspond to the ROM and RAM sizes for the RX MCU that you have selected for the project.

Suitable Products
CS+ (formerly CubeSuite+)
C/C++ Compiler Package for RX Family